DRV.IZERO

Description

This parameter sets the current that is used during the DRV.ZERO procedure.

General Information

Type

NV Parameter

Units

Arms

Range

Drive peak current to 0 Arms

Default Value

0 Arms

Data Type

Float

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5085h/0

M_01-00-00-000

Related Topics

DRV.ZERO

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen