DRV.NAME

Description

You can assign a unique name to any drive under the following conditions:

  • Only use ASCII characters
  • Max length of 10 characters
  • No spaces in name

This name is one way to identify the drive in a multiple drive network (for instance, in a TCP/IP network on which multiple drives reside).

From the terminal screen, DRV.NAME returns the name of the drive as ASCII characters.

 

General Information

Type

NV Parameter

Units

N/A

Range

N/A

Default Value

No-Name

Data Type

String

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

2031h/0

M_01-00-00-000

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen