DRV.RUNTIME

Description

DRV.RUNTIME returns the length of time that the drive has been running since it was first activated. This time includes the current session and the total amount of time from all previous sessions.

General Information

Type

R/O Parameter

Units

Days:Hours:Minutes:Seconds

Range

N/A

Default Value

N/A

Data Type

String

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

2011h

M_01-00-00-000

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen