DRV.TEMPERATURES

Description

DRV.TEMPERATURES reads the temperature in different parts of the drive (power and control boards). The temperature is read from temperature sensors located in the drive.

Example

Below is an example of the output for this command :

Control Temperature: 39 °C

Power1  Temperature: 31 °C

Power2  Temperature: SensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer does not exist.

Power3  Temperature: Sensor does not exist.

General Information

Type

R/O Parameter

Units

°C

Range

55 to 125 °C

Default Value

N/A

Data Type

String

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3610h/0

3611h/0

M_01-00-00-000

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen