DRV.VERIMAGE
Description
DRV.VERIMAGE reads the versions of the different images in the drive. This parameter returns the version data from each image .i00 file.
Example
Below is an example of the output for this parameter:
------------------------------------
Resident Firmware: R_0-0-11
Operational Firmware: M_0-0-15
Resident FPGA"Field-Programmable Gate Array" FPGA is a semiconductor device that can be configured by the customer or designer after manufacturing; hence the name "field-programmable": FPB004_0001_00_07
Operational FPGA : FP0004_0001_00_07
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Start Version |
M_01-00-00-000 |
|
Copyright © 2018 Kollmorgen |
|