FBUS.PLLTHRESH

Description

This parameter sets number of successful synchronized cycles needed to lock the PLL.

General Information

Type

NV Parameter

Units

N/A

Range

0 to 10,000

Default Value

0

Data Type

Integer, U32

See Also

Appendix B: FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Manuals

Start Version

M_01-00-00-000

Fieldbus

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

50B1h/0

M_01-00-00-000

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen