FBUS.SYNCACT
Description
This parameter reads actual distance from the desired sync distance.
General Information
|
Type |
R/O Parameter |
|
Units |
ns |
|
Range |
0 to 250,000 ns |
|
Default Value |
0 ns |
|
Data Type |
Integer, U 32 |
|
See Also |
Appendix B: FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Manuals |
|
Start Version |
M_01-00-00-000 |
|
Fieldbus |
Index/Subindex |
Object Start Version |
|---|---|---|
|
3496h/2 |
M_01-00-00-000 |
|
Copyright © 2018 Kollmorgen |
|