GUI.DISPLAY

Description

This parameter reports to the GUI"Graphical User Interface" A GUI is a type of user interface which allows people to interact with a computer and computer-controlled devices what the drive currently is displaying. For all GUI commands, the data is compressed and formatted for the GUI, not for the user.

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Display

See Also

N/A

Start Version

M_01-00-00-000

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen