IL.DFOLDT
Description
IL"Instruction list" This is a low-level language and resembles assembly.DFOLDT is the time constant of the exponential drop (foldback) of the current towards the drive continuous current.
General Information
|
Type |
R/W Parameter |
|
Units |
s |
|
Range |
1 to 65.535 s |
|
Default Value |
Usually 2.500 s, but may change according to the drive type. |
|
Data Type |
Float |
|
See Also |
Foldback |
|
Start Version |
M_01-00-00-000 |
|
Copyright © 2018 Kollmorgen |
|