IL.FOLDFTHRESH

Description

IL"Instruction list" This is a low-level language and resembles assembly.FOLDFTHRESH is the fault level of the current foldback algorithm. If IL.IFOLD drops below the value for IL.FOLDFTHRESH, then a fault is generated and the drive is disabled.

To avoid reaching the current foldback fault level, set IL.FOLDFTHRESHU well below the continuous current value for both the drive and the motor or set the IL.FOLDFTHRESHU value to zero.

General Information

Type

R/O Parameter

Units

Arms

Range

0 to 500 Arms

Default Value

Drive peak current (DRV.IPEAK)

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3420h/0

M_01-00-00-000

Related Topics

Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen