IL.KACCFF
Description
This value sets the gain for the acceleration feedforward (a scaled second derivative of the position command is added to the current command value) .
This parameter is valid only in the position mode (DRV.OPMODE = 2).
General Information
|
Type |
R/W Parameter |
|
Units |
mArms/(rad/s²) |
|
Range |
0 to 39113.288 mArms/(rad/s^2) |
|
Default Value |
0 mArms/(rad/s²) |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3426h/0 |
M_01-00-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|