IL.KPLOOKUPINDEX

Description

This parameter sets the index into the Current Loop Gain Scheduling Table. The table is 256 records long, spanning 0 A to 1.62 * DRV.IPEAK.

To determine the level of current that corresponds to a table index, use the following equation:

IL"Instruction list" This is a low-level language and resembles assembly.CMD = (Table Index /157) * DRV.IPEAK

General Information

Type

R/W Parameter

Units

N/A

Range

0 to 255

Default Value

0

Data Type

Integer

See Also

IL.KPLOOKUPVALUEIL.KPLOOKUPVALUESIL.KP

Start Version

M_01-04-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5265h/0

M_01-04-00-000

Related Topics

Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen