IL.MFOLDT
Description
IL"Instruction list" This is a low-level language and resembles assembly.MFOLDT sets the time constant of the exponential drop (foldback) of the current towards motor continuous current.
General Information
|
Type |
R/O Parameter |
|
Units |
s |
|
Range |
0.1 to 2,400 s |
|
Default Value |
10 s |
|
Data Type |
Float |
|
See Also |
Foldback |
|
Start Version |
M_01-00-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|