IL.OFFSET
Description
This value is added to the overall current loop feedforward value.
General Information
|
Type |
RW Parameter |
|
Units |
A |
|
Range |
|
|
Default Value |
0 A |
|
Data Type |
Float |
|
See Also |
IL.FF |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3423h/0 |
M_01-00-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|