IL.VVFB

Description

The range for this parameter depends on whether the drive model is an MV/240 VAC or an HV/480 VAC. 

The VBusScale parameter sets the drive model:

MV/240 VAC:  VBusScale = 1

HV/480 VAC:  VBusScale = 2

VBusScale is used for multiple parameter ranges that are model dependent, such as IL"Instruction list" This is a low-level language and resembles assembly.KP.

General Information

Type

R/O Parameter

Units

V

Range

–1200*VBusScale to +1200*VBusScale

Default Value

N/A

Data Type

Integer

See Also

IL.VUFB

Start Version

M_01-00-00-000

Related Topics

Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen