MOTOR.TEMP

Description

This parameter returns the motor temperature, which is represented as the resistance of the motor's PTC or NTC.

General Information

Type

R/O Parameter

Units

Range

0 to 232

Default Value

N/A

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3612h/0

M_01-00-00-000

Related Topics

Motor | MOTOR.RTYPE

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen