PL.FBSOURCE

Description

This parameter determines the feedback source that the position loop uses. A value of 0 for this parameter selects the primary feedback, a value of 1 selects the secondary feedback. If you use the secondary feedback as the source for the position loop, then FB2.MODE mode should be set as 0 (A/B signals). A/B signals are the only supported feedback type as secondary feedback into the position loop. Other settings for FB2.MODE are intended as pulse inputs or a gearing command when PL.FBSOURCE remains 0.

0

Primary Feedback connected to X10.

1 Secondary Feedback (DRV.HANDWHEEL) connected to X7 or X9.
2 Tertiary Feedback connected to X9 (only supported with AKD-x-xxxxx-NBxx-xxxx).

General Information

Type

NV Parameter

Units

N/A

Range

Range will differ depending on drive model.
0 to 1 (for AKD-x-xxxxx-NAxx-xxxx)
0 to 2 (for AKD-x-xxxxx-NBxx-xxxx)

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5128h/0

M_01-00-00-000

Related Topics

PL.ERR | PL.ERRFTHRESH | PL.ERRMODE | PL.ERRWTHRESH

Position Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen