REC.TRIGPARAM
Description
REC.TRIGPARAM sets the parameter on which the recorder triggers.
This parameter is only used when REC.TRIGTYPE = 2.
Input values are:
- One of the set drive parameters list that can be set as a trigger. The available parameters for trigger are: PL.ERR , PL.CMD, PL.FB, VL.CMD, VL.FB, IL"Instruction list" This is a low-level language and resembles assembly.CMD, and IL.FB.
- Internal value or variable of the drive (same as for DRV.MEMADDR input).
General Information
|
Type |
R/W Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
IL.FB |
|
Data Type |
String |
|
See Also |
REC.TRIG |
|
Start Version |
M_01-00-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|