REGEN.WATTEXT

Description

Sets the regen resistor's power fault level for an external regen resistor (when REGEN.TYPE = -1).

Above this fault level, the regen resistor's PWM wil be 0 and a fault will be issued.

General Information

Type

R/W parameter

Units

W

Range

0 to 62,000 W

Default Value

1000 W

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3414h/0

M_01-00-00-000

Related Topics

Regeneration

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen