VL.FF

Description

This parameter displays the velocity loop overall feedforward value.

General Information

Type

R/O Parameter

Units

Depends on or

Rotary: rpm, rps, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, µm/s, (custom units)/s

Range

0 to VL.LIMITP

Default Value

0

Data Type

Float

See Also

VL.KBUSFF

Start Version

M_01-00-00-000

Related Topics

Velocity Loop

VL.KVFF

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen