VL.GENMODE
Description
This parameter is used to select the velocity generator mode.
|
Mode |
Description |
|---|---|
|
0 |
d/dt mode: The derivative of the mechanical angle of the drive is fed to a first order low pass. |
|
1 |
Luenberger Observer mode |
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
51B0h/0 |
M_01-00-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|