VL.OBSMODE
Description
This parameter sets the observer operating mode. When VL.OBSMODE = 0, the observer is not part of the control loop; that is, VL.FB is used as the velocity feedback signal to the velocity loop. When VL.OBSMODE = 1, the observer is part of the control loop; VL.MODEL is used as the velocity feedback signal.
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-03-00-004 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
51BBh/0 |
M_01-03-00-004 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|