DTATPLCopen motion icon

Function BlockA function block groups an algorithm and a set of private data. It has inputs and outputs. - Generate a pulse at given date and time

Inputs

YEAR : DINT     Wished year (e.g. 2006)
MONTH : DINT    Wished month (1 = January)
DAY : DINT      Wished day (1 to 31)
TMOFDAY : TIME  Wished time
RST : BOOL      Reset command

Outputs

QAT : BOOL      PulseWhen the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated signal
QPAST : BOOL    True if elapsed


  • The real-time clock may not be available on all controller hardware models. Please consult the controller hardware specifications for real-time clock availability.

Remarks

Parameters are not updated constantly. They are taken into account when only:
- the first time the block is called
- when the reset input (RST) is TRUE
In these two situations, the outputs are reset to FALSE.

The first time the block is called with RST=FALSE and the specified date/stamp is passed, the output QPAST is set to TRUE, and the output QAT is set to TRUE for one cycle only (pulse signal).

Highest units are ignored if set to 0. For instance, if arguments are "year=0, month=0, day = 3, tmofday=t#10h" then the block will trigger on the next 3rd day of the month at 10h.

In FFLD language, the block is activated only if the input rung is TRUE..

ST Language

(* MyDTAT is a declared instance of DTAT function block *)
MyDTAT (YEAR, MONTH, DAY, TMOFDAY, RST);
QAT := MyDTAT.QAT;
QPAST := MyDTATA.QPAST;

FBD Language

FFLD Language

(* Called only if EN is TRUE *)

IL Language:

(* MyDTAT is a declared instance of DTAT function block *)
Op1: CAL MyDTAT (YEAR, MONTH, DAY, TMOFDAY, RST)
FFLD  MyDTAT.QAT
ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal  QAT
FFLD  MyDTATA.QPAST
ST  QPAST

See also

DTEVERY   Real time clock functions

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen