LOWORD
Inputs
IN : UDINT 32 bit register
Outputs
Q : UINT Lowest significant word
Remarks
In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.
In IL"Instruction list" This is a low-level language and resembles assembly, the input must be loaded in the current result before calling the function.
ST Language
Q := LOWORD (IN);
FBD Language
FFLD Language
(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
IL Language:
See also
LOBYTE HIBYTE HIWORD MAKEWORD MAKEDWORD
|
Copyright © 2018 Kollmorgen |
|