ANY_TO_SINT / ANY_TO_USINT
Inputs
IN : ANY Input value
Outputs
Q : SINT Value converted to a small (8 bit) integer
Remarks
For BOOL input data types, the output is 0 or 1. For REAL input data type, the output is the integer part of the input real. For TIME input data types, the result is the number of milliseconds. For STRING inputs, the output is the number represented by the string, or 0 if the string does not represent a valid number. In FFLD language, the conversion is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung. In IL"Instruction list" This is a low-level language and resembles assembly Language, the ANY_TO_SINT function converts the current result.
ST Language
Q := ANY_TO_SINT (IN);
FBD Language
FFLD Language
(* The conversion is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
IL Language
Op1: FFLD IN
ANY_TO_SINT
ST Q
See also
ANY_TO_BOOL ANY_TO_INT ANY_TO_DINT ANY_TO_LINT ANY_TO_REAL ANY_TO_LREAL ANY_TO_TIME ANY_TO_STRING
|
Copyright © 2018 Kollmorgen |
|