AS-interface Functions
ASiReadPP |
read permanent parameters of an AS-i slave |
ASiWritePP |
write permanent parameters of an AS-i slave |
ASiSendParam |
send parameters to an AS-i slave |
ASiReadPI |
read actual parameters of an AS-i slave |
ASiStorePI
|
store actual parameters as permanent parameters |
-
-
AS-i networking may be not available on some targets. Please refer to OEM"Original equipment manufacturer" A term that refers to containment-based re-branding, namely where one company uses a component of another company within its product, or sells the product of another company under its own brand. OEM refers to the company that originally manufactured the product instructions for further details about available features.
Interface
Params := ASiReadPP (Master, Slave);
bOK := ASiWritePP (Master, Slave, Params);
bOK := ASiSendParam (Master, Slave, Params);
Params := ASiReadPI (Master, Slave);
bOK := ASiStorePI (Master);
Arguments
Master : DINT Index of the AS-i master (1..N) such as shown in configuration
Slave : DINT Address of the AS-i slave (1..32 / 33..63)
Params : DINT Value of
AS-i parameters
bOK : BOOL TRUE if successful
|
Copyright © 2018 Kollmorgen |
|