ASIN / ASINLPLCopen motion icon

FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Calculate an arc-sine.

Inputs

IN : REAL/LREAL  Real value

Outputs

Q : REAL/LREAL   Result: arc-sine of IN

Remarks

In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.

In IL"Instruction list" This is a low-level language and resembles assembly, the input must be loaded in the current result before calling the function.

ST Language

Q := ASIN (IN);

FBD Language

AsinFbd.gif (1165 octets)

FFLD Language

(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
AsinLd.gif (1410 octets)

IL Language:

Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  IN
     ASIN
     ST  Q    (* Q is: ASIN (IN) *)

See also

SIN   COS   TAN   ACOS   ATAN   ATAN2

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen