BIN_TO_BCDPLCopen motion icon

FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Converts a binary value to a BCD (Binary Coded Decimal) value

Inputs

IN : DINT  Integer value

Outputs

Q : DINT   Value converted to BCD
           or 0 if IN is less than 0

Truth table (examples)

IN Q

-2

0 (invalid)

0

0

10

16 (16#10)

22

34 (16#22)

Remarks

The input must be positive. In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.

In IL"Instruction list" This is a low-level language and resembles assembly, the input must be loaded in the current result before calling the function.

ST Language

Q := BIN_TO_BCD (IN);

FBD Language

FFLD Language

(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)

IL Language:

Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them         IN
     BIN_TO_BCD
     ST         Q

See also

BCD_TO_BIN

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen