Handling Exceptions

The compiler enables you to write your own exception programs for handling particular system events. The following exceptions can be handled:

In the sub-program that handles the exception you can perform any safety or trace operation. You then have the selection between the following possibilities:

Handlers can also be used in DEBUG mode for tracking the bad operation. Just put a breakpoint in your handler. When stopped, the call stack will show you the location of the division in the source code of the program.

Startup Exceptions

You can write your own exception program to be executed before the first application cycle is executed:

  1. Create a new main program that will handle the exception. It cannot be an SFC"Sequential function chart" It can be used to program processes that can be split into steps. The main components of SFC are: - Steps with associated actions - Transitions with associated logic conditions - Directed links between steps and transitions program.
  2. In the editor of global defines, insert the following line:
#OnStartup ProgramName

  • Warning: The program is executed before all other programs within the fisrt cycle. This implies that the cycle timing can be longer during the first cycle. You cannot put breakpoints in the Startup program.

Shutdown Exceptions

You can write your own exception program to be executed after the last application cycle when the runtime system is cleanly stopped:

  1. Create a new main program that will handle the exception. It cannot be an SFC program.
  2. In the editor of global defines, insert the following line:
#OnShutdown ProgramName

  • Warning: You cannot put breakpoints in the Shutdown program.

Division By Zero Exceptions

You can write your own exception program for handling the "Division by zero" exception. Below is  the procedure you must follow for setting an exception handler:

  1. Create a new sub-program without any parameter that will handle the exception
  2. In the editor of global defines, insert the following line:
#OnDivZero SubProgramName

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen