NOT_MASK
Inputs
IN : ANY Integer input
Outputs
Q : ANY Bit to bit negation of the input
Remarks
Arguments can be signed or unsigned integers from 8 to 32 bits.
In FFLD language, the input rung (EN) enables the operation, and the output rung keeps the same value as the input rung. In IL"Instruction list" This is a low-level language and resembles assembly language, the parameter (IN) must be loaded in the current result before calling the function.
ST Language
Q := NOT_MASK (IN);
FBD Language
FFLD Language
(* The function is executed only if EN is TRUE *)
(* ENO is equal to EN *)
IL Language:
See also
|
Copyright © 2018 Kollmorgen |
|