Power Rails
The power rail on the left represents the TRUE value and initiates the rung state.
Power rails can also be used in FBD"Function block diagram" A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks language. Only Boolean objects can be connected to power rails.
See also
|
Copyright © 2018 Kollmorgen |
|