Enter notes for steps and transitions
- entering Level 2 for steps
- entering Level 2 for transitions
Notes can be displayed in the chart. The last button of the toolbar enables you to switch between possible displays:
| Swap between possible overviews of level 2 in
the level 1 chart: |
Notes have no meaning for the execution of the chart. Entering notes for steps and transitions enables you to enhance the auto-documentation of your programs. It also provides an easy way to write and exchange specifications of an SFC program before actions and conditions are programmed.
|
Copyright © 2018 Kollmorgen |
|