SFC Steps
-
-
To change the number of a step, transition or jump, select it and hit Ctrl+ENTER keys.
All actions linked to the steps are executed according to the activity of the step.
| Inactive step | Active step |
|
|
|
In conditions and actions of the SFC program, you can test the step activity by specifying its name ("GS" plus the step number) followed by ".X".
For example:
|
GS100.X |
is TRUE if step 100 is active (expression has the BOOL data type) |
You can also test the activity time of a step, by specifying the step name followed by ".T". It is the time elapsed since the activation of the step. When the step is deactivated, this time remains unchanged. It will be reset to 0 on the next step activation. For example:
|
GS100.T |
is the time elapsed since step
100 was activated (expression has the TIME data type) |
Initial steps
Initial steps represent the initial situation of the chart when the program is started. There must be at least one initial step in each SFC chart. An initial step is marked with a double line:
|
Copyright © 2018 Kollmorgen |
|