ST / IL Syntax coloring

The ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal / IL"Instruction list" This is a low-level language and resembles assembly editor supports syntax coloring according to the selected programming language (ST or IL). The editor uses different colors for the following kinds of words:

  1. Default (identifiers, separators)
  2. Reserved keywords of the language
  3. Constant expressions
  4. Comments

  • Reserved words such as function names are blue. Subprograms including Kollmorgen UDFBs are not reserved and will show as black.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen