Tooltips in the ST / IL Editor

During test (connected mode or simulation) of the program, the ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal / IL"Instruction list" This is a low-level language and resembles assembly Editor shows in a tooltip the current value of the variable pointed to by the mouse cursor. You don't need to run any specific command to open the tooltip. Just put the mouse on the variable symbol and wait for one second.

The value shown in the tooltip is automatically refreshed while the tooltip is open.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen