Known Issues

Defect Description
BZ-10072 Conversion from LREAL to PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML fixed point numbers loses precision
BZ-9975 KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger crashes in the Workbench Performance Servo Tuner Window
BZ-9928 ESI file list is not updated when good and bad ESI files are added at the same time
BZ-9848 KAS IDE broken if Windows user name contains non-ascii characters
BZ-9835 Non-ASCII characters in projects not handled properly in the KAS IDE
BZ-9834 Import/export from/to non-ascii file names does not work correctly
BZ-9832 Cannot add libraries (.KAL files) with non-ASCII file names
BZ-9496 AKD-N firmware download fails if 4x drives are selected
BZ-8608 KAS IDE views do not scale if Windows text scaling is > 100%
DT-3442 PDO objects not defined in the object dictionary (or 24bit size) will not work properly with MLSmpXxxxx(...) functions
DT-3439 KAS IDE hangs if AKD variable added to watch window before opening AKD-GUI"Graphical User Interface" A GUI is a type of user interface which allows people to interact with a computer and computer-controlled devices. To work-around, open the AKD-GUI (Configuration tab) first.
DT-3431 PLCopen move blending with jerkIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time. If the blending move is commanded with an unreachable velocity, the move may abruptly decelerate to the final position within one sample, exceeding the specified deceleration rate.
DT-3427 E21 when KAS IDE running O-Scope is disconnected
DT-3419 Adding ESI File After Scanning Results in No Selected PDOs
DT-3418 PLCopen S-Curve move may not reach target with small JerkIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time
DT-3417 EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs scan fails after a AKD drive firmware download failure with a wrong EtherCAT topology
DT-3410 Recovered projects don’t recover imported libraries (.kal files)
DT-3408 When a crash report fails due to error (ex - timeout, connection failure, …) report is lost. User cannot resend.
DT-3382 MLInitTrig does not configure the AKD Capture engine correctly for a negative edge trigger.
DT-3367 ECAT network restore fails to recover from drive FW download failure.
DT-3290 PDOs need padding to meet byte boundary requirement. The IDE PDO Editor does not automatically pad PDOs on non-byte boundaries. The problem can be avoided by manually adding dummy objects to pad the PDO size to line-up on byte boundaries. For more details, see the article on KDN (kdn.kollmorgen.com/content/how-do-i-insert-pdo-padding-kas-pdo-editor).
DT-3287 KL3314 Operation. Temperature values are not calibrated properly to the thermocouple. To work-around the problem, use ECATWriteData to setup the control word (16xE0) and send value (16x2006) to Register R32 and a second ECATWriteData to write zero (0) to the control word to set up the continual output of the temperature.
DT-3265 ModbusModBus is a serial communications protocol and is now the most commonly available means of connecting industrial electronic devices. ModBus is often used to connect a supervisory computer with a remote terminal unit in supervisory control and data acquisition (SCADA) systems. Versions of the ModBus protocol exist for serial port and Ethernet (it is widely used with TCP/IP over Ethernet) renumber address does not work with String variables. In the FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Editor Modbus configurator, if you right click input registers and choose the renumber address option, it will make the addresses overlap.
DT-3041 Missed cycles while doing file operations
DT-3013 Modified cam file is not downloaded when forcing an Online Change.
DT-2940 WebBrowser component not working for TxB panels
DT-2935 K-Bus slices analog inputs Offset parameter does not work
DT-2798 IDE disconnects from the controller after several days(
DT-2590 Breakpoint with For(…) loop, increases VM load significantly
DT-2560 IDE animation with non-matching project versions
DT-2523 On windows 7 Home Premium Edition on HP computers, there is a known issue when using the simulation.
To work around this issue, we have to delete the Platform system variable:
DT-1134 IDE always reports the project has been modified

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen