Service Motion

Service Motion allows you to set up simple motion (Command Source must be set to Mode 0 - Service). It is typically used during initial set up to exercise the system. It can be used to help troubleshoot the system, execute tuning, make repetitive moves for verification of mechanical set up, or for other general simple motion needs. There are multiple ways to set up motion depending on the desired result in torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist, velocity or position modes. In all modes, you can run a momentary pulse, set up reversing motion, or initiate continuous motion.  

The chart below identifies the commands available on the Sevice Motion view:

Button or Dialog Box

Description

Available in OP Mode

PulseWhen the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated

Alternates between the commanded current or velocity and zero velocity. You can specify the time period between the commanded value and the return to zero. Setting a time to zero will generate a continuous command.

TorqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist, Position, Velocity

Reversing

Alternates between the two commanded values. You can specify the time the command will be held in each state.

Torque, Position, Velocity

Continuous

Runs the commanded current or velocity continuously.

Torque, Position, Velocity
Group Selects parameter group to be used with service motion. Group 1 selects parameter group for SM.MODE 0, and group 2 selects parameter group for SM.MODE 2. See SM.MODE for more details. Torque, Position, Velocity
Current 1/Current 2 Only shows while drive is in Torque mode. Sets the two different currents. Torque

Velocity 1/Velocity 2

Only shows while drive is in Velocity or Position mode. Sets the two different velocities.

Velocity, Position

Time 1/Time 2

Sets the time for which the different commands are generated. Setting a time to zero generates a continuous command.

Velocity, Position

Start/Stop

Starts and stops the motion.

Torque, Position, Velocity
Acceleration Sets the acceleration ramp for service motion if set to greater than 0. Velocity, Position
Deceleration Sets the deceleration ramp for service motion if set to greater than 0. Velocity, Position
Accel. Limit The acceleration limit set by DRV.ACC . Velocity, Position
Decel. Limit The deceleration limit set by DRV.DEC . Velocity, Position

Position Feedback

Displays the present position of the motor.

Torque, Position, Velocity

Velocity Feedback

Displays the present velocity of the motor.

Torque, Position, Velocity
Current Feedback Displays the present current of the motor. Only displays when drive is in Torque mode. Torque

Related Parameters

SM.I1

SM.I2

SM.I2

SM.MOVE

SM.T1

SM.T2

SM.V1

SM.V2

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen