Settings

Navigation Tree

The Settings view allows you to configure the drive to fit your specific application. When you click Settings in the navigation pane located to the left of the WorkBench screen, additional views for configuring your drive appear. By default, only settings applicable to your current drive operation mode and command source will appear in this tree. To show all settings available for the AKD (even if the these settings are not used with the current operation mode and command source), right click on Settings and select Show all Settings.

Settings View

From the main Settings view, you can configure the following drive settings:

Button or Dialog Box

Description

Command Source

Selects where the command is being provided:

0-Service: Communicate with the drive using the TCP/IP service channel.

1-FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design: For normal KAS RuntimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running operation

0-Service : For tuning and commanding motion via the AKD setup screens

Operation Mode

Selects the servo loops that are used in the drive.

Mode 0: Current Loop (used primarily during drive setup)

Mode 1: Velocity and Current Loops (used primarily during drive setup)

Mode 2: Position, Velocity, and Current Loops (Default KAS Runtime mode)

Related Topics

Using Command Source and Operating Modes for details on configuring the drive for your application.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen