Function BlockMLAxisStopPipe Network motion icon

Description

Stop with the specified deceleration.

After stopping the drive, you need to restart the motion by realigning the actual position with the reference position

The purpose of the MLAxisStop Command is not to remove the input source, but to stop the drive from continuing to move.

When the stop occurs, the master keeps moving and the axis starts ignoring the Pipe Position value and begins a controlled stop based on the input parameters. Also at that point, any Axis Block level profile (issued from FB like MLAxisAbs, MLAxisRel...) are aborted. When the stop is complete, it is up to the application to decide how to move the axis, master, or both to a position where they can be realigned, and the master restarted (see more details about the Restarting Motion here).

The realign function is used to move the axis to a restart position in order to enable synchronized machine motion to start again. Once the realign function is successfully completed, the Pipe Position is again summed with the Generator Position to create the Reference Position. See more details here.

Arguments

Input

ID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

Start

Description

 

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

—

Deceleration

Description

 

 

Data type

LREAL

 

Range

—

 

Unit

User unit/sec2

 

Default

—

Output

Default (.Q)

Description

Comes true when the Axis is completely stopped. See State Machine here.

See more details here

 

Data type

BOOL

 

Unit

n/a

PipePos

Description

Corresponds to the Pipe Position input to the axis at the time the stop is triggered.

 

Data type

LREAL

 

Unit

User unit

GenPos

Description

Corresponds to the Generator Position input to the axis at the time the stop is triggered.

 

Data type

LREAL

 

Unit

User unit

RealignPos

Description

Realign Position is the Reference Position at which the stop is triggered. The Realign Position is obtained by converting the last value sent to the drive from drive interface units into user units.
The Realign Position is useful if you want to return to the point at which the trajectory was abandoned, or in case you need to realign the master to the slave.

 

Data type

LREAL

 

Unit

User unit

StopPos

Description

Corresponds to the last Reference Position sent to the drive at the time when the Axis is completely stopped (see State Machine here). It is functionally different than the Actual Position because that position is the drive position converted to user units.

The correct delta for the realign move to get in sync with the trajectory in order to realign the slave to the master is the current Reference Position minus the Stop Position for the realign move. After stopping, if the axis is disabled and the motor position is manually altered, this distance must be taken into account when performing the realign.

 

Data type

LREAL

 

Unit

User unit

Related Functions

MLAxisReAlign

Example

Structured Text

Inst_MLAxisStop(PipeNetwork.AXIS1, bStop, 200000);
If Inst_MLAxisStop.Done Then
Axis1_PipePosition := Inst_MLAxisStop.PipePos;
Axis1_GeneratorPosition := Inst_MLAxisStop.GenPos;
Axis1_RealignPosition := Inst_MLAxisStop.RealignPos;
Axis1_StopPosition := Inst_MLAxisStop.StopPos;
End_if;

Ladder Diagram

Function Block Diagram

MLAxisStop: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen