MLFB_HomeFindLimitInputThenZeroAngle
Description
Similar to the Find Input Limit method, the find input limit then find zero angle. Mode follows the same steps, but upon completion of the move, it continues to move to find the zero angle reference of the motor.
Arguments
Input
|
ibExecute |
Description |
Start homing, edge-triggered |
|
Data type |
BOOL |
|
iAxisID |
Description |
ID of Axis block of Pipe Network |
|
Data type |
BOOL |
|
iPosition |
Description |
Reference position |
|
Data type |
BOOL |
|
ibDirection |
Description |
0=positive, 1=negative |
|
Data type |
BOOL |
|
iVelocity |
Description |
Reference speed |
|
Data type |
BOOL |
|
iAcceleration |
Description |
Reference acceleration |
|
Data type |
BOOL |
|
iDeceleration |
Description |
Reference deceleration |
|
Data type |
BOOL |
|
ibLimitSwitch |
Description |
Pos. or neg. limit switch, high-active (depends on ibDirection) |
|
Data type |
BOOL |
|
iTimeout |
Description |
Time monitoring (T#0ms: off) |
|
Data type |
BOOL |
Output
|
obDone |
Description |
Done bit |
|
Data type |
BOOL |
|
obActive |
Description |
Active bit |
|
Data type |
BOOL |
|
obError |
Description |
Error bit |
|
Data type |
BOOL |
|
oErrorID |
Description |
Error identifier, see list here
|
||||||||||||
|
Data type |
DINT |
Example
ST
//Call homing function on Axis1 with preset velocity, accel, and decel values
//Start in negative direction and stop when axis hits limit switch or times out
//after seeing limit switch, moves to zero angle and set axis position to zero
Inst_MLFB_HomeFindLimitInputThenZeroAngle( StartHomeRoutine,
PipeNetwork.AXIS1,
0,
TRUE,
100,
1000,
1000,
HomeDigitalInput,
T#30s );
HomeDone := Inst_MLFB_HomeFindLimitInputThenZeroAngle.obDone;
Function Block Diagram
FFLD
|
Copyright © 2018 Kollmorgen |
|
[Top]