MLFB_PlsTimeFw
Description
This function block should be used in the command position path with ascending position. A dedicated comparator pipe block is needed. The Boolean output oPLS is set to TRUE if the position of the comparator has crossed the start position and a timer with iOnTime is started. When the timer has expired the output is set to FALSE. The function block is executed cyclically. The modulo position is considered. The function block has the possibility to compensate a delay time of the connected device, e .g. glue nozzles.
Arguments
Input
|
ibExecute |
Description |
Enable PLS |
|
Data type |
BOOL |
|
|
iDedicatedCmpID |
Description |
ID of dedicated comparator |
|
Data type |
DINT |
|
|
iStartPos |
Description |
Start position of PLS |
|
Data type |
LREAL |
|
|
iOnTime |
Description |
Time PLS is on |
|
Data type |
TIME |
|
|
iDelayTime |
Description |
Delay time for compensation |
|
Data type |
TIME |
|
|
ibForce |
Description |
Force PLS |
|
Data type |
BOOL |
Output
|
oPLS |
Description |
Position limit switch |
|
Data type |
BOOL |
Example
Timing
ST
//PLSOutput is True when chosen comparator passes 180 for 3 seconds a T#2ms delay
//Can also force the output to be true with ForceOuput variable
Inst_MLFB_PlsTimeFw( EnablePLS, PipeNetwork.COMPARATOR, 180, T#3s, T#2ms, ForceOutput );
PLSOutput := Inst_MLFB_PlsTimeFw.oPLS;
FBD
FFLD
|
Copyright © 2018 Kollmorgen |
|
[Top]