SD Card Path Conventions
To access the SD card memory a valid SD card label must be used at the beginning of the path, followed by the relative path to the SD card. (Valid SD Card Label)/(Relative Path)
A valid SD card relative path starts with //, /, \\, or \. This is immediately followed by SDCard which is followed by \ or /. Please note that this path label is case insensitive.
| Valid Paths | Notes |
|---|---|
| //SDCard/file1 | |
| \Sdcard/dir1/file1 | dir1 must have been already created |
| /sdcard/dir1/file1 | dir1 must have been already created |
| //sdCard\file1 |
| Invalid Paths | Reason for being invalid |
|---|---|
| ///SDCard/file1 | Started with more than two forward or backward slashes |
| /\Sdcard/dir1/file1 | Started with one forward and one backward slash |
| /sdcarddir1/file1 | No forward or backward slash |
| /sdcard1/dir1/file1 | Invalid label |
In order to maintain compatibility with the Simulator, the SDCard folder is created inside the userdata folder . File access points to userdata/SDCard when a PDMM SDCard path is used on the Simulator.
See Also:
|
Copyright © 2018 Kollmorgen |
|