udpSendToPLCopen motion icon

Description

This function sends UDP data to a server.

Arguments

Input

En Description Execute the function
  Data type BOOL
  Range [0,1]
  Unit n/a
  Default —
sock Description ID of the client socket
  Data type DINT
  Range [0,+65535]
  Unit n/a
  Default —
nb Description Number of bytes of data to send
  Data type DINT
  Range [0,65535]
  Unit n/a
  Default —
add[] Description Buffer containing the UDP address
  Data type USINT
  Range [0,32]
  Unit n/a
  Default —
data Description The characters to send
  Data type STRING
  Range [0,255]
  Unit n/a
  Default —

Output

OK Description Returns true when the function successfully executes. See Function - General rules.
  Data type BOOL
  Unit n/a

Examples

Structured Text

bUdpSendTo := udpSendTo(Socket_Number,5,add,'1000'); 

Ladder Diagram

Function Block Diagram

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen