Drives
This section details the following
| AKD part number | Description |
|---|---|
| AKD-B00106 | 120/240 VAC 1.5A Drive |
| AKD-B00306 | 120/240 VAC 3A Drive |
| AKD-B00606 | 120/240 VAC 6A Drive |
| AKD-B01206 | 120/240 VAC 12A Drive |
| AKD-B02406 | 120/240 VAC 24A Drive |
| AKD-B04806 | 120/240 VAC 48A Drive |
| AKD-B00107 | 240/480 VAC 1.5A Drive |
| AKD-B00307 | 240/480 VAC 3A Drive |
| AKD-B00607 | 240/480 VAC 6A Drive |
| AKD-B01207 | 240/480 VAC 12A Drive |
| AKD-B02407 | 240/480 VAC 24A Drive |
| AKD-N00307 | 3A Distributed Servo Drive |
| AKD-N00607 | 6A Distributed Servo Drive |
For further information on drives, refer to the following manuals:
| Drives Guide | Description | |
|---|---|---|
| AKD Quick Start |
|
Contains all information needed to safely install and setup an AKD drive |
| AKD PDMM Installation Manual |
|
Covers the most important points to install the drive hardware and software Provides instructions for basic drive setup and connection to a network |
| AKD User Manual |
|
Describes how to use your drive in common applications. It also provides tips for maximizing your system performance with the AKD |
| AKD2G Installation Manual |
|
|
| AKD Accessories Manual |
|
Includes technical data and dimensional drawings of accessories such as cables, brake resistors, and mains supplies |
| AKD EtherCAT Manual |
|
Describes the installation, setup, range of functions, and software protocol for the EtherCAT |
| AKD2G EtherCAT Manual |
|
|
| S300 Reference Documentation |
|
Kollmorgen website that gives access to all S300 |
| S700 Reference Documentation |
|
Kollmorgen website that gives access to all S700 |
Table 9-6: List of Drive Manuals
-
-
The AKD manuals are located under:
C:\Program Files\Kollmorgen\AKD WorkBench 1.0.x.y\WebHelp
(x.y must be replaced with the version number)
(this location differs if you chose another location when installing AKD).
-
-
Refer to our Web site for up-to-date information and material that are available in the Automation Component Solutions section.
Note that you first need to log in before accessing KAS Literature.
-
-
Depending on the number of AKD drives physically present in the EtherCAT network, the KAS IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger might slow down when getting data.
The KAS Runtime
In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time).
Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running is not concerned with this limitation.
|
Copyright © 2018 Kollmorgen |
|