Connect Remotely

You can connect to a AKD PDMM or PCMM from an external network using VPN or other tunneling protocol. To do so you must open the following ports which are used by KAS to connect to a controller.

Port Component/Protocol using the port
80 KAS IDEClosed"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger: Controller Web Server; Download PLC application; Runtime front end communication. This is necessary for the connection to the runtime.
502 HMI and other Modbus devices to communicate with Modbus TCP.
2222 Ethernet/IP communication
4002 KAS IDE: Oscilloscope variable monitoring.
4003 KAS IDE: Communication with the PLCClosed"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Virtual Machine. This is necessary for the connection to the runtime.
9900 KAS IDE: Communication with the runtime engine; WorkBenchviews. This is necessary for the connection to the runtime.
34962 Profinet communication
34964 Profinet communication
44848 Ethernet/IP communication

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen