Architectural View

The diagram shows an architectural view of what KAS is from a hardware and software perspective, or realtime and not-realtime components. Hardware is shown in blue shaded boxes and, minimally consists of a computer, a controller, one or more drives, I/O, and optionally an HMIClosed"Human-machine interfaces " Also known as computer-human interfaces (CHI), and formerly known as man-machine interfaces, they are usually employed to communicate with PLCs and other computers, such as entering and monitoring temperatures or pressures for further automated control or emergency response device. Each of these components has a software aspect, many of which communicate with other components. Communication may be done over EthernetClosedEthernet is a large, diverse family of frame-based computer networking technologies that operate at many speeds for local area networks (LANs) or HTTP (seen in blue), EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs (seen in green), ModbusClosedModBus is a serial communications protocol and is now the most commonly available means of connecting industrial electronic devices. ModBus is often used to connect a supervisory computer with a remote terminal unit in supervisory control and data acquisition (SCADA) systems. Versions of the ModBus protocol exist for serial port and Ethernet (it is widely used with TCP/IP over Ethernet) (seen in red), or several other protocols.

Figure 2-8: Architectural view of KAS components.

The non real-time part is composed of:

Item Description
KAS IDEClosed"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger The development tool which allows creating the project (i.e. design, create and run virtually)
KAS RuntimeClosedIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running ...
KVB The development tool which allows creating an HMI interface.
HMI Available when integrated on a Programmable Automation Controller platform (not present when integrated a programmable drive)

The realtime components, including that which run the KAS Runtime engine, consists of:

Item Description
IECClosed"International Electrotechnical Commission" IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 virtual machine Responsible for managing an IEC 61131-3 application with its programs and variables
Motion manager Manages motion engines, axis objects and motion bus drivers.
The KAS Runtime comes with two motion engines: Pipe Network and PLCopen.
The motion engine implements different motion algorithms and functions to create, access and delete pipes, pipe blocks and axes (e.g. MLPNAxisCreate, MLGearInit, MLPipeAct).
It also provides a set of Functions and Function Blocks that IEC 61131-3 applications can use to control the behavior of these algorithms
I/O manager Manages I/Os and I/O drivers. It works closely with the VM Manager instances to map transparently all IEC 61131-3 variables declared as input or output
Motion Bus A plug-in giving access to the EtherCAT network
custom function blocks A plug-in implementing custom function blocks

Interface between the realtime and non-realtime systems is done via shared memory buffers.

The Runtime communicates with the KAS IDE during operation to:

  • Receive further instructions from the KAS IDE such as a direct motion command
  • Provide status information to the KAS IDE for motion and operation of the application program
  • Provide information displayed on the KAS IDE scope
  • Provide Log information to the KAS IDE

  • When the KAS Runtime is implemented with a programmable drive, the interface between the real-time and non real-time parts is done via Ethernet based on TCP/IP protocol.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen