PDMM or PCMM Rotary Switch

The rotary switch on the AKD PDMM or PCMM can be set on a position from 0 to 9.

Switch Position Description
Position 0 The drive tries to get an IP address from a DHCP server. If the DHCP fails, then the AKD PDMM or PCMM uses AutoIP to get a usable IP address.
Position 1 The default custom static IP address, 192.168.0.101 or a custom IP address.
Position 2-9 The AKD PDMM or PCMM is pre-configured with static IP addresses ranging from 192.168.0.102 (Position 2) to 192.168.0.109 (Position 9).

  • If a DHCP server is not present, the drive will assume an Automatic Private IP Address of the form 169.254.x.x


  • The AKD PDMM or PCMM will not set (or show) an IP address without an attached network cable.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen