AXIS_REF Structure

The PLCopenClosedA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML specification indicates a data structure to be used for identifying the axis at a function block input. AXIS_REF contains two members:

Member Type Description
AXIS_NUM INT The axis number
AXIS_ENGINE UINT Reserved. Do not modify this variable or rely on its value.

For more details on Axis Number, About Axis Name and Number

You have to create and initialize this data structure in your application. See usage examples provided in Function Blocks Description.

Concept Link IconSee Also

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen