Functions
IEC
"International Electrotechnical Commission"
IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies has defined standard functions and also allows you to create your own functions (called user-defined functions). Typically, functions take several inputs and return a single output as the result of processing.
- Standard functions are for example ADD (addition), ABS (absolute), SIN (sine), COS (cosine), GT (Greater Than),….
- User-defined functions, as in the following example, can be used repeatedly once defined.
FUNCTION SIMPLE_FUN : REAL VAR_INPUT A, B : REAL; C : REAL := 1.0; END_VAR SIMPLE_FUN := A*B/C; END FUNCTION
|
Copyright © 2018 Kollmorgen |
|