Application Status Bar

The tooltip of the application status bar gives more information about the application stored in the target: name of the project, name of the device, version of the application, its build number and date of compilation.

To view the tooltip, hold the mouse over the application status bar and wait for 1 or 2 seconds without moving the mouse.

Device Tooltip displays Version

Figure 5-57: Device Tooltip displays Version

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen